Part Number: LM5122
Other Parts Discussed in Thread: LM51772
Tool/software:
Hi team,
We are designing a high-power LED flash system. The LEDs require 500W peak power for a 1ms pulse, with a flash frequency ranging from 1Hz to 67Hz. We plan to use a MOSFET to switch the LEDs and are looking for a suitable regulator to supply this power. Using two drivers in parallel is acceptable if needed.
The output requirements are either 50V at 10A or 100V at 5A, with an input voltage range of 9V to 36V. We are currently evaluating the LM5122 and LM5172 using Webench.
Is this design feasible? Could you recommend any suitable power devices or alternative approaches for this application?
LM5122 - webench.ti.com/.../SDP.cgi
LM5172 - webench.ti.com/.../SDP.cgi
Thanks,
Jagan