This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS564247: Layout check for tps564247 buck converter + ground layout

Part Number: TPS564247


Tool/software:

Hello,

please check the layouts i suggest:

layout 1: https://imgur.com/KosJpPj

layout 2: https://imgur.com/KmwgNLv

in layout 1, the big polymer cap is not facing the same direction as other parallel ceramics, so it shares the + terminals with them but its ground is on the other side. While in layout 2 all the same direction.

the parallel caps are very close to the inductor and the regulator chip ground pin as seen in images.

input caps are also facing their positive pads together for the input power of 15v but their grounds are sideways due to low space. i can fix this  but prefer if this is fine.

everything is done correctly in terms of effective capacitance, input caps, i added big input clc filters too, i added output protection and reverse blockage via 2 mosfets, etc... so only the layout is what i need help with.

another important issue is the ground pins of the output connector... they may not be directly connected to the right side regulator due to space. however there will be lots of via on those ground pins and all around output caps and chip to ensure very smooth way to ground.

design is 4 layers with last 3 are solid ground pours.

i guess the loop for both regulators is good and short, but the ground pins of the output and the source ground pin are not very close... will this be an issue? i mean, there are many ground pours and stuff...

please check and advise.