Tool/software:
HELLO
I am trying to build a 12V 5A 60W power supply using the UCC28710. As shown in my schematic, I calculated all component values based on the datasheet recommendations. However, I’m facing an issue: the output voltage is only 10V, and the output current is limited to 0.5A when measured with a multimeter in series with the load.
I experimented by changing the current sense resistor (Rcs) to 0.15Ω, which allowed the current to increase to 1.5A. However, based on the equations from the datasheet, I calculated that for a 5A output, I should be using an Rcs of 0.35Ω.
here is vdd of the ic
V aux before diode
VS PIN
MOSFT GATE