Tool/software:
Please tell me how to design a planar transformer for a DC/DC flyback converter for
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Please tell me how to design a planar transformer for a DC/DC flyback converter for
Hi Alexander,
Thanks for reaching out! TPS23734EVM is 5V active clamp forward converter. Please see design parameters suggestions for different topologies:
5V forward transformer:
Turns ratio SEC : PRI : AUX = 1 : (4–6) : (2–2.8)
Lm = 90–165 µH, Isat > 1.5 A
12V forward transformer:
Turns ratio SEC : PRI : AUX = 1 : (1.8–3) : (0.9–1.1)
Lm = 90–165 µH, Isat > 1.5 A
5V flyback transformer:
Turns ratio SEC : PRI : AUX : BIAS = 1 : (5–9) : (2–2.8) : (1–1.2)
Lm = 50–150 µH, Isat > 2.6A @ Npri_min & Lm_min
12V flyback transformer:
Turns ratio SEC : PRI : AUX : BIAS = 1 : (2–3.5) : (0.9–1.1) : (0.4–0.6)
Lm = 50–150 µH, Isat > 2.6A @ Npri_min & Lm_min
Best regards,
Diang