This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650362-Q1: Checking for the design availability - TPS65036x-Q1

Part Number: TPS650362-Q1

Tool/software:

Hi 

Good day !

The client's design will consider using the following power supply.

3.3V / 1A
2.5V / 300mA or above
1.8V / 1A
1.2V / 300mA or above

Could you please help confirm whether the TPS65036x-Q1 series is applicable?
Or can you recommend other more suitable products ?

Thank you !

  • Hello Eason,

    Buck1 can support an output of 3.3V and 2A. Buck2 and Buck3 can support an output of 1.8V and 1.2V up to 2.7A. 

    The TPS65036x-Q1 can support an output of 2.5V and up to 300mA with the Low Noise LDO. However, if the load will be greater than 300mA, an external LDO would be needed.

    Best regards,
    Jude Stehling