Other Parts Discussed in Thread: TUSB1146-Q1, TUSB1146, TUSB564-Q1, TUSB1064-Q1
Tool/software:
In TPS25763-Q1 datasheet "8.3.3 External NFET and LSGD" section, it describes TPS25763-Q1 is a DisplayPort sink device and operates as a Dual Role Power (DRP) port using the application configuration GUI default settings, does this mean the TPS25763 can only be used as a sink devices?
I'm working on DisplayPort Alternate Mode over USB-C, in order to realize the host side can be connector to the projector, I plane to use TUSB1146-Q1+TPS25763-Q1 in the host port,but I don't know if this is feasible, I worried that the TPS25763-Q1 can only be used as a sink port, not a source port.
Please let me know if there is any problem with my solutin?
Thanks!