This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74700D-Q1: Ideal diode/ORing controllers recommendation

Guru 11140 points
Part Number: LM74700D-Q1

Tool/software:

Hello,

My client is looking for an ORing controller solution that supports the following conditions:

  - ORing of two 12V Power Rails

  - Max VIN : 18V or higher

  - IOUT: 2.5A or higher

  - The lower the Rds(on), the more preferred

  - Recommended with external MOSFET

Please recommend the most suitable product among TI products.

Thank you.

JH