This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65219: Power-up behavior when PB keeps low on TPS6521902.

Part Number: TPS65219


Tool/software:

Hi,

If customers start power-up with Push_button_Low on TPS6521902, TPS6521902 goes power-down on 8ms later.  Is it correct?   Please let us know.

Thanks and best regards,
M.HATTORI.

  • Hi Hattori-san,

    The behavior looks correct to me but a scope capture would be more helpful showing the actual pin status while device powers up.

    For TPS6521902, FSD (first supply detection) is enabled, so the device initiates the power up sequence regardless of the PB pin status but if the pin status is changed prior to ACTIVE state or in ACTIVE state then holding it low for 8s would cause the device to power down.

    Sathish