Tool/software:
I would like to parallel two of the +/-15 volt output devices. The data sheet says this:
8.4.2.3 Connecting the DCV01 in Parallel
If the output power from one DCV01 is not sufficient, it is possible to parallel the outputs of multiple DCV01s,
as shown in Figure 8-9 (applies to single output devices only). The synchronization feature allows easy
synchronization to prevent power-rail beat frequencies at no additional filtering cost.
What would be the problem paralleling the dual output devices? I have bread boarded it and it does function, but I fear there is a dragon hiding around the corner.
Thank you!
Charlie