This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27523: UCC27523 OUTA to INB, looks like Shorted

Part Number: UCC27523


Tool/software:

Hi

Try to using UCC27523 as a half-duplex, single-wire communication bus (2 channels not enable at same time), but it not working. looks like Pin 7 & 4 shorted to the GND, any help ? Thanks

  • Hi Chu,

    Can you answer a few of these questions:

    1. What is the Com bus?
    2. What is the failure rate?
    3. Have you done an ABA analysis?
    4. When did this failure occur, and do you have the waveforms before the failure?
    5. Do you have any waveforms of a good unit of start-up, steady state, shut down?

    Thanks,

    Suzuko

  • Thanks 

    1. Just a inverted (idle LOW) single-wire UART

    2. Just prototype to replace SN74LVC2G240DCTR that no enough drive ability

    3. No ABA

    4. just prototype: Even both channel are disable, the pin 7 & 4 is about 15 ohm

    5. never get it working 

  • Understanding the Problem

    UCC27523 Overview

    • OUTA (pin 7) and OUTB (pin 5) are independent push-pull outputs capable of sourcing/sinking ±2.5A.

    • INB (pin 4) is a logic input, not designed to sink or source current.


    Warning️ What Went Wrong

    If you connected OUTA (pin 7) to INB (pin 4) or tried to "loop" the outputs for half-duplex communication:

    • OUTA can source/sink large current, which can destroy INB, which is a high-impedance logic input.

    • INB might now be internally damaged or shorted to GND due to this overcurrent.


    X Why This Won’t Work

    • UCC27523 is a gate driver, not a bus transceiver.

    • It's meant to drive MOSFET gates, not signal lines with possible contention or bidirectional behavior.

    • There’s no output tri-state capability — outputs are always push-pull active, which is dangerous in a shared line.

  • yes ChaGPT is correct: When Channel disable, it is not Z

  • UCC27523 is a gate driver, not a bus transceiver (not working)

  • Hi Chu,

    I'm glad you figured things out. Our device is not meant for bidirectional behavior as it is meant to directly drive the MOSFET.

    If you have any further questions, please feel free to reach out.

    Thanks, 

    Suzuko Devine