This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546E25: D-CAP4 제어기와 D-CAP+ 제어기 비교 문의

Part Number: TPS546E25
Other Parts Discussed in Thread: TPS544E27

Tool/software:

SoC core 전원용 IC를 검토하고 있습니다.
TI 부품 TPS546E25와 TPS544E27 사용을 고민하고 있는데,
D-CAP4 제어기와 D-CAP+ 제어기가 각각 사용되고 있습니다.
core 전원에 더 적합한 제어기가 어떤 것인지 알 수 있을까요?
혹시 두 가지 제어기의 dynamic 특성을 비교한 자료가 있을까요?
  • Hello,

    Based on translation tool, I am understanding that you are comparing TPS546E25 & TPS544E27 to select.
    Both devices have their own advantages. TPS544E27 is D-CAP+ while TPS546E25 is D-CAP4.

    TPS544E27:

    • 40A current limit
    • 30mm^2 package 6x5
    • Iq: 9000uA

    TPS546E25:

    • 50A current limit
    • Stackable
    • 30mm^2 package 6x5
    • Iq: 7500uA

    TPS544E27: https://www.ti.com/product/TPS544E27#params

    TPS546E25: https://www.ti.com/product/TPS546E25#params

    I attached both product folders above which compare the two devices. It will depend on what you are looking for specifically, whether it is fast transient response, efficiency, stackable, current limit, etc

    Thank you,

    Calan