Other Parts Discussed in Thread: TPS61022
Tool/software:
Hi,
Im using TPS61230 in a project. Basically it is used to power a device that is always connected. When I set the enable pin, the Vout of the TPS61230 stays at 1.8-1.9V. I believe the issue is due to the fact that the TPS61230 cant finish the start up due to a possible heavy load connected, because if I enable it without the load connected and connect the load later the output gives me the 5V needed.
If this is the case how can I solve this ? Do you have any other part that is more suitable for heavy loads ? Can I use a load switch at the output of TPS61230, so i can wait for it to startup and later enable the power for the other device ?
Thank you!