Tool/software:
Is the inductance 8.2uH appropriate in the figure? According to the data manual, 4.7uH is appropriate in boost mode but 4.7uH is small in buck mode, so I chose 8.2uH.
The design parameters are
input voltage: 6~18V
output voltage:12V
output current limit:2.5A
switching frequency:405kHz