This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27427: Primary Charge Termination Algorithm & Taper Rate

Part Number: BQ27427


Tool/software:

Hello, 

The conditions of Primary Charge Termination Algorithm and Taper Rate are not quite clear. Please clarify the following:

  1. In the Table in 7.4.2.3.10, the Taper Rate unit is defined as "0.1 h rate" but below the Taper Rate is compared with IRateAvgx. 
    1. Is the Taper Rate dimension Time (h)? If not, what is the correct dimension of the Taper Rate?
    2. What is the dimension of the  IRateAvgx?
  2. The second requirement to qualify for Primary Charge Termination is:
    "During the same periods: Accumulated change in capacity per 40-second period"
    but this doesn't contain any requirement. What is the requirement related to "Accumulated change in capacity"?

Best regards,

Vadim