Tool/software:
This here is a general question in design of boost converter. In the document slva372d it is mentioned that the output capacitor is calculated as Cout = (Iout*D)/F *delta(V). I understand that delta(V) here is the ripple voltage. Is this delta(V) the rms ripple or peak to peak ripple value.
For eg: if i have a requirement for the rms output ripple to be 50mV then can i directly plug this into the equation or have to find the peak to peak value and insert into the equation?