Other Parts Discussed in Thread: TPS61169,
Tool/software:
Hello E2E Experts,
Good day.
I'm building a project with your TPS611655DBVR driver. It is powered by a 4.2V battery. The 4p6s LED matrix is powered with the required current of 180mA and 16V. But the driver does not regulate the current, I connect the multimeter to the matrix plus and SW plus and get an unstable current depending on the input voltage. Please help me solve the problem. CTRL is connected via 10kOhm to +5V input.
Regards,
TICSC