This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z746: bq27z746

Part Number: BQ27Z746
Other Parts Discussed in Thread: BQSTUDIO, BQ27Z558

Tool/software:

Hello,
I'm currently working with the BQ27Z746 fuel gauge, but it is not connecting to BQStudio. The fuel gauge does not output voltage even when connected to the device.
Even while charging, the gauge does not connect.

It was working fine at first, but after flashing the image in BQStudio (which showed "0/0" during the process), it never connected again.

Previously, with the BQ27Z556, I was able to resolve a similar issue by fully discharging the battery and then recharging it, which allowed BQStudio to reconnect.
However, this approach does not work for the BQ27Z746.

Please, I would really appreciate any help or guidance on how to recover the device.

I'm using BQStudio version 1.3.127.