Tool/software:
Hello,
My costumer has a question on the Reverse polarity protection (RPP) functionality of the HSS:
Does this substitute the need of a Reverse polarity protection IC (LM74xx-Q1 + Fet or diode) ?
Is the load that follwos the HSS protected from a Reverse Polarity event ?
Based on my understanding this feature protects only the device itself but not the load or whatever come after the HSS.
In case the device can substitute a classical RPP does it meets all automotive ISO7637 transient requirements?
It seems that based on the DS this supports only a part of the requirement of the ISO7637 (test 2?)
Thanks,
Oscar