This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22810: Two devices in OR-ing configuration

Genius 17525 points
Part Number: TPS22810
Other Parts Discussed in Thread: TPS2121

Tool/software:

Hi Experts,

Good day.

Would like to ask if it is possible to use two TPS22810 devices in an ORing configuration. One power source is a 3S9P battery ranging from 9V to 12.6V, while the other is a fixed 12V supply.

Thank you.

Regards,
Archie A.

  • Hello Archie,

    You need reverse current blocking for Oring controller.

    TPS22810 doesn't have Oring.

    What's the current rating you are looking for?

    I will assign the thread to my colleague who supports ID and Oring.

    Thanks

    Amrit 

  • Hi Amrit,

    Customer shared info:

    TPS2121 power mux, but unfortunately its quiescent current is too high (up to 400 µA). Are there any power muxes available with lower quiescent current? 
    One power source is a 3S9P battery ranging from 9V to 12.6V, while the other is a fixed 12V supply. The maximum load current is 1A.

    Thank you.

    Regards,
    Archie A.

  • Hi Archie,

    You can consider using LM74700 which will prioritize the higher voltage available. You will not have control over which power rail to use.

    Regards,

    Shiven Dhir