Tool/software:
Dear Ti_e2e Team,
This is Kurata.
I would appreciate it if you could answer the following questions.
Electrostatic discharge tests were conducted on prototype power supply knit products using this device.
When static electricity was applied to the front panel of the power supply unit, the IC's 1-second shutdown protection circuit malfunctioned, temporarily halting power output before restarting.
This malfunction undesirably triggered an alarm lamp and an alarm signal from the power supply system.
Since this system is designed for continuous operation, a malfunction caused by static electricity could not be tolerated.
As a countermeasure, we increased the capacitance of the filter capacitors on the BLK and Isns pins of the UCC256403 and shorted the BW pin to GND to disable overvoltage protection, but this did not improve the reset phenomenon observed during the electrostatic discharge test.
Furthermore, to prevent electrostatic noise from entering, we strengthened the filtering by inserting a low-resistance resistor (10 Ω) or ferrite bead near the Vcc pin's printed wiring pattern, and by inserting a ferrite bead near the GND pin's pattern.
However, the results showed almost no improvement, and we are unable to come up with an effective solution as we are unable to identify the route through which the noise that is causing the IC to malfunction is entered, so we are at a loss as to what to do.
Please let us know the cause and mechanism behind the malfunction caused by this electrostatic discharge test, as well as any fundamental ways to improve the situation.
Thank you in advance for your consideration.