This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

redundant power supply for non ATCA blades chassis.

Other Parts Discussed in Thread: TPS2456, TPS24710, TPS2410

Hi

I Need  a fail safe, 100% available power as long as at least one of the power sources is available(see attached)

When both supplies available prefer to have load sharing and reduce the output power of each supply.

load is 25A with 9mF bulk capacitance

I was thinking about the TPS2456 as a solution but not sure if it the most suitable one.

please advise

Thanks in advance for the support

 

12V_paralleling.pdf