Other Parts Discussed in Thread: TPS65131,
Tool/software:
Hello, I am looking for some advice on power distribution.
I am building an audio installation, and I need to power our "devices" in groups of 6. The devices are usually powered by 5V from a USB-C connector, and each draw a maximum of 0.3A. There are TPS65131 converters on the input of the devices, similar to the generic schematic in the datasheet.
I would prefer not to use a USB power hub and instead power them from a 15V rail which I already have for other signals which are also being sent to the devices. The cables will be approximately 3 meters long though. My idea was to use a single Buck converter like LMR14030 to create the 5V rails, and then distribute the 5V lines to the devices over 3 Meter cables. These are audio devices so low noise is important, but the devices already have somewhat good filtering with LDOs following the TPS65131. The "Backup" outputs are just for reserve in case I want to add 2 more devices.
So my questions.
- Is a single LMR14030 (or similar) a good solution for powering all 6 devices, or would it be better for each of the 8 outputs to have their own lower power buck converter?
-
What type of filtering (if any) should I put on the PSU outputs? I currently just put in some ferrite beads, but I would appreciate some help on how to thoughtfully design that part.
- Would an LDO after the LMR14030 be a good idea since I want to minimise noise?
Thanks!