This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62084: tlv62084dsgr

Part Number: TLV62084


Tool/software:

I'm using this for 3.3v to 1.5v conversion. My active load current is 800mA. why is my Vos pin getting short with ground, what are the different reasons it could happen?

  • Hi Harish,

    Can you probe the inductor current and input voltage with the load on to see that both are as expected? Average inductor current should correspond to the load current.

    My feeling is either there is too much load on the output or the input voltage has gone below UVLO.

    Best regards,

    Varun