This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM82866A: some questions

Part Number: TPSM82866A

Tool/software:

Hi team,

Q1. When they use the device at forced PWM mode, VSET/MODE pin needs to be high. How do you usually make the pin high after the device has started up? Could you also give the example schematic for this?

Q2. Could you tell the current value when the device will enter PSM at the condition below? 

TPSM82866AA0SRDJR

input voltage : 5V

output voltage : 3.3V

Q3. in the datasheet, the output voltage can be +/-2%, but the condition when the accuracy becomes +/-2% is not sure. Could you tell more detailed condition when the accuracy becomes +/-2%?

Regards,

Noriyuki Takahashi