Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:

Hi JDJ,
Regarding 1, both input MUX FETs can be turned off using REG0x12[7] even with valid voltage at VACx. Regarding 2, there is no way to turn off the internal battery FET diode. Some customers have added an external PFET, with pull up resistor and NFET gate driven by GPIO if battery >1S, to disconnect the battery from BAT pin.
Regards,
Jeff
So with a valid I2C command we can stop power to the system from the VBUS line even if that means the IC and system completely lose power (without a battery case). Would the IC come back up and default on or would we need battery power to allow the system to send the I2C message and turn us back on again?