Tool/software:
Hi ,
I need help to review my attached schematic. Its BQ24210 based Power management circuit which would process the solar PV panel primarily to charge the 3.7V li-ion Battery and also its power the Load. For emergency backup, added USB power adapter input as well incase of no battery and no solar panel but still aimed to power the load.
The buck converter output USWP +3.3V will be connected to Microcontroller. So Microcontroller will be powered always
The switched power output SWP +3.3V will be connected to 4G module to power it on need basis, decided by the microcontroller
Kindly review all the passive components and its ranges and give the feed back.
Looking forward to hear from you all...
Thanks,
Prabakaran