Tool/software:
Dear TI experts,
My customer asked about power on reset in fault situation. Could you check these questions?
1. In the table 6.9 of the datasheet there are lists of fault situation.
There are auto recovery faults and also faults which need to be reset manually.
Is it okay to do power on reset in all fault situations although some faults are auto-recoverable?
(Because my customer do not use I2C so they do not know what fault occur exactly, so they want to always do power on reset.)
2. Is it okay to control PWM signal by main MCU, and I2C communication is connected to sub MCU which is in monitor module?
In that case, They need to communicate via I2C (sub MCU in the monitor) while PWM is controlled by MCU which is outside the monitor.
Please check these 2 issues. Thanks.
Best regards,
Chase