Tool/software:
Hi Team
We are working with TPS54202, the input given to it is 28V and required output is 24V, 2A
Requesting to check the attached screenshot and let us know the changes, also please let us know the values of R577, R578
Tool/software:
Hi Team
We are working with TPS54202, the input given to it is 28V and required output is 24V, 2A
Requesting to check the attached screenshot and let us know the changes, also please let us know the values of R577, R578
Hi Avishek,
Recommended Operating Conditions for EN pin max is 7V.
As your input voltage is 28V, you can use R577 = 51k and R578 = 5k for Enabling the IC.
Schematic seems accurate assuming the Inductor you are using L81 = 22uH.
Best Regards,
Usha.
Hi Usha,
1)Here we are converting 28V to 24V , i wanted to know if 2A is enough for the conversion.
2) Also, I Request you to provide graphs of efficiency and load regulation with input 28V.
Hi Manogna,
Since you have raised another ticket will follow up in that.
We will close this thread.
Best regards,
Usha.