This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3429: Major power loss and high thermal dissipation when using LM3429

Part Number: LM3429

Tool/software:

Hi TI Team,

We are currently using the LM3429MH/NOPB LED driver in a design with the following configuration:

  • Input Voltage: 12V (up to 8A available)

  • LED Configuration: 20 LEDs in series (each with Vf ≈ 3.0V)

  • LED Current: 200 mA

  • Estimated Output Voltage: ~60V

  • Switching MOSFET: 100V Vds, 5A Id rated

  • Output Diode: Properly selected for voltage and current ratings

  • Compensation Network: Tuned according to TI guidelines

We are observing significant power loss, with efficiency dropping below 50%, and the system is experiencing major thermal dissipation issues. The board heats up considerably even with good passive selection and proper layout. We've confirmed that our LC filter, OVP, UVP, and other standard protections are implemented as per the datasheet recommendations.

Despite optimizing the compensation network and component selection (including inductor and sense resistor), the problem persists. Increasing the LED current beyond 200–250 mA with output voltage hovering around 58V leads to excessive heat buildup, damaging passive components in some cases and even triggering thermal shutdown in the LM3429.

We would appreciate your support in identifying potential causes for this inefficiency and guidance on resolving this thermal issue. Is this behavior expected in such a setup, or is there any critical design consideration we might be missing?

Looking forward to your insights.

  • Hi, 

    Can you share the schematic? Also, can you share the tested waveform? I'd like to see voltage of pin IS , GATE, and inductor current. 

    Also, if you have thermal camera, you may scan the board to see hot spot. 

    Let me know which passive component is damaged during your test?