Other Parts Discussed in Thread: LP5522, , TPS92610EVM,
Tool/software:
Hello,
My customer would like to blink and LED at 0.5Hz (1 second on and one second off). They do not want to use I2C, and would prefer a resistor for setting current and another pin for controlling PWM / on-off status. They were using the LP5522 device but had an issue where the drive signal was being interpreted by the 1-wire interface and getting stuck in an undesirable state.
Could they use the PWM pin as just constant low (completely off), and constant high (full output current) to blink the LED at 0.5Hz? Ibeleive this is okay, but want to double check. None of the graphs or parametric tables talk about 0% duty cycle, but there is one line in the datasheet that says "PWM input can be adopted for LED brightness adjust and LED ON/OFF control."
Please confirm, and thanks!
John