This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24040: Does BQ24040 support setting charging temperature

Part Number: BQ24040

Tool/software:

Dear TI Engineer,

We have one question about the charging temperature of BQ24040. That is, the battery was integrated a 10KNTC which corresponds to a B value of 3435. If we directly connect the TS pin to the NTC line of the battery, charging will stop below 0°C and above 60°C. Is that correct?

Now we want to set the charging temperature to the range of 0°C to 45 °C, which means that BQ24040 will stop charging below 0°C or above 45 °C. How do we set it? Can you give us some suggestion for this application?

Thanks,

Kind Regards