Tool/software:
Hi,
I'm running into an issue with the TPS566231RQFR where about 10% of the time, it shorts VIN to GND upon the first power up. This has been an issue with various load connected as well as with all load disconnected from the output. We're using a 14-16V Vin input and this issue has occurred with it current limited to 2A. The schematic implementation exactly follows Webench and the layout closely matches the recommended layout as well. The issue is difficult to reproduce- when we swap the chip on a "bad" board for a fresh chip, we do not see the issue again.