This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS568215: Do you have other parts having OOB feature ?

Part Number: TPS568215
Other Parts Discussed in Thread: TPS56A37, TPS56838

Tool/software:

Hi Sir,

I am looking for buck DC-DC converters which support OOB function. 

Please help to suggest parts supporting the below requirements.

1. VIN = DC12V and DC24V

2. Vout = 5V

3. Iout = 8A -10A

4. OOB or any features can protect against overvoltage conditions, there is another power source that is slightly higher than Vout.

TPS568215 can meet the requirement but its VIN range cannot support DC24 applications.

Thanks.