Other Parts Discussed in Thread: TPS92641
Tool/software:
Hi Sirs,
I want to confirm the speed at which the LED driver can turn on and off the IRLED current.
Do boost and buck-boost modes have the same performance?
I expect that when PWM pulse = low, the LED current should be zero (like Figure 8-14 and 8-16 in the datasheet).
However, the measured results in EVM look like PWM dimming cannot achieve fast dimming. The LED current is switched off and on slowly (please see Figure 5-7, Figure 5-8 and Figure 5-9 in the EVM User's Guide)
I also found that the LED ripple current is a little bit high (please see Figure 8-2 in the datasheet). I am afraid that high ripple current will cause image quality issues.
Can the ripple current be reduced to below 20mA ?
Thanks.