This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5023: Protection ajustment LM5023

Part Number: LM5023

Tool/software:

Hi!

I have a SMPS project ... , I was reading the datasheet and I had doubts about the calculations of R1, R2, R_external and R_sense.

I need to determine over current and over voltage protection ... from what I can understand... R1, Rsense, Rexternal are related to starting current, while R2 is related to overvoltage? Is this correct?

I'm using it on R2 2k2, R1 23k7... on Rsense 0.43R and on Rexternal 374R ... 

My output is 6.3V, and I'm noticing that for every 100mA I increase my load (up to 1.3A), I need to increase my input by 10VAC... for example:

Input 64VAC, load 400mA, when starting, the output pulsates, indicating protection. It starts after increasing my 10VAC (74VAC) input ...