This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25145: Regarding the evaluation module (EVM) for evaluating the LM25145.

Part Number: LM25145
Other Parts Discussed in Thread: LM5145, LM5146

Tool/software:

Hi team,

I searched for an EVM for the LM25145 but couldn't find one.

When checking the product folder, the LM5145EVM is recommended for purchase.

Since the LM5145 is a similar IC, I plan to proceed with evaluation using the LM5145EVM.

The main difference between the LM25145 and LM5145 is the input voltage range, and I believe their configurations are essentially equivalent, correct?

Also, the output voltage of the LM5145EVM is set to 5V.

By changing the feedback resistor divider ratio, it should be possible to verify operation at "input 24V → output 21.5V, 7A," correct?

Best regards,

Kyohei