Tool/software:
Hello
I have implemented this DCDC to generate a -5.4V output. The source is a very stable 3.3V output from a DCDC (with 3A max output) .
I really copied the design from the datasheet more or less. No magic here.
The output load is 30mA only! The load is an LDO to generate -5V for an analog circuit.
The EN signal comes 14ms after the 3.3V is stable.

I have now 21 boards of which 8 boards have a failure on this DCDC.
They all show a very similar behaviour:
I see +0.65V on the output. The 10R VIN resistor has a drop of about 1.5V, leaving about 1.7V at the VIN. So the current going into VIN is about 150mA.
So I assume this IC is dead.
Could be anything else than ESD be the reason? Can pre-bias kill this IC? We are using sometimes this board with no load attached for R&D reasons.
The COMP cap C107 and 220nF from VREF C102 are totally at the PCB edge. So when you hold the PCB with your fingers on the edge, you will touch those caps.
We do have ESD shoes etc, but not an ESD floor.
Is it known that this IC is so super sensible?
Thanks for any inputs! I really don't know what else it could be, but almost 50% failure is too high to just say "it's ESD" it seems.