This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24179: Looking for a Lithium-Ion battery charger

Part Number: BQ24179
Other Parts Discussed in Thread: BQ25730

Tool/software:

Hello,

My customer is looking for a buck-boost Lithium-Ion battery charger for the following requirements. They are thinking around BQ24179 now but they would like to hear TI expert opinion. What BQ devise does TI think best for their requirements?
  Input voltage VIN: 9V to 25.2V
  Output voltage Vo/IO: 16.8V/2.3A
  Operating mode: What can be operated on the output CCCV
  Output connected load: Lithium-ion battery (Nominal voltage: 14.8V, charge voltage/current: 16.8V/2.3A)
  Switching element: Both internal FET type and external type can be used
  Shape: As small as possible.

Best regards,

K.Hirano