This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24640: Looking for a buck converter for super-cap load

Part Number: BQ24640


Tool/software:

Hello,

My customer is looking for a buck converter for super-cap load for the following requirements. They are thinking around BQ24640 now but they would like to hear TI expert opinion. What BQ devise does TI think best for their requirements?
   Input voltage VIN: 9V to 25.2V
   Output voltage Vo/IO: 5V/1-10A
   Operating mode: CCCV
   Output connection loads: Super Capacitor and DC/DC converter
   Switching element: Both internal FET type and external type can be used
   Size: As small as possible.

Best regards,

K.Hirano