This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76972: Initial BQ76972 Programming Using EV2400, no REG1 REG2 Output

Part Number: BQ76972
Other Parts Discussed in Thread: EV2400,

Tool/software:

Hello, I am powering BQ76972 with 48V total stack, 3.0V per cell and communicating over I2C with the EV2400 module. I am externally powering REG1 with 3.3V while I try to program the BQ76972. I am able to read all the cell voltages correctly, so I believe I have active communication with the BQ76972. I am simply trying to set REG1 and REG2 to be enabled and both be 3.3V. 

I am trying to set REG12 to 0xDD, and REG0 to 0x01. This should enable both and set the each LDO to 3.3V. 

However, I will write both of these registers to the BQ, and both DO NOT get enabled. 

I have upgraded the EV2400 FW to the latest (v0.32). 

Are there specific steps that I am missing? I have UNSEALED the BQ and SET_CFGUPDATE. 

REGIN stays at 3.0V the whole time.