BQ27542EVM: Ambient temperature of 45°C, SOC% error

Part Number: BQ27542EVM

Tool/software:

Hi Sir, 

At an ambient temperature of 45°C, What is a reasonable value of SOC% error?
The battery voltage is 3.77V, the remaining capacity is about 600mAh, the cell capacity is 2830mAh, and the chemID is 3839.

Thank you.

  • Hello,

    Your question has been assigned and will be reviewed when possible. In the meantime could you attach the .log and .gg files associated with the project.

    Thank you,
    Alan

  • If everything is tuned correctly (including load prediction - the answer depends on how accurate the load prediction is, which also depends on the load), then we can typically achieve +/-3 percentage points reports SOC - true SOC calculated after the discharge/charge (using measured coulomb count and total passed charge).