This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31710: INH/UVLO for 10V

Part Number: LMZ31710


Tool/software:

Hi

I have a input coming to LMZ31710. I want to use UVLO such that when the input is stable 10V then only my LMZ31710 should be active.
If not it should disable the regulator can I do that.


Regards,
Raju