Part Number: BQ76952
Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
Hi team,
We are using BQ76952 AFE to read cell measurements.
We are able to read cell volt measurements properly, but the current measurement is not reading properly. The shunt resistor value is 0.5 milli ohms.
When we are applying 1 A, it is reading 65. So, We changed the following register values in the AFE.
CC gain for 0.5mohm shunt : 14.9536(Little endian (IEEE-754) value 41 6F 41 F2)
Capacity gain for 0.5mohm shunt :Little endian (IEEE-754) value 6A 1C 08 4B
DA configuration register value changed to 0x06.
However the value is still showing 65 for 1A and 134 for 2A respectively.
Kindly help us to resolve the issue.
Best regards,
Hareesh