This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1685: E-fuse for low side battery negative

Part Number: TPS1685
Other Parts Discussed in Thread: TPS1663, TPS2663,

Tool/software:

Hi,

We are looking for a way to protect the return line to our low voltage batteries (2x 12V 7Ah) in the scenario where the positive line is shorted to chassis and bypasses the protection we have on the high side.

An e-fuse would be a great solution but I am not sure if it is possible to use it on the low side, since the integrated MOSFET would see 0V rather than 24V at its input.

If we decouple the power input (IN) from the IC power supply (VDD) and power the IC from our other supply, can we use the e-fuse on the ground line back to the batteries?

Thank you for your help!