With regards to an application using the bq20z75:
- During a Qmax update can it be expected that in some cases Qmax_1 and Qmax_2 would update but Qmax_3, Qmax_4 and Qmax_Pack would remain the same? And other combinations as well?
- One of the Qmax update requirements is to pass a given amount of charge (37%). If charge starts at 63% and then at 92% percent jumps to 100% by achieving primary charge termination would that still qualify as 37% passed charge? It technically only passed 29 percent then jumped to 100%.