This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23730: current limit design

Part Number: TPS23730


Tool/software:

Hi Team,

The input adopts a shunt design with two sets of inputs, 30W and 50W

50W for other adapters

30W is powered by POE

POE design Vin = 54V, Vout=12V,Iout=2.5A

Can the output be controlled to maintain 2.5A output?

  • Hi Allen,

    Thanks for reaching out! 

    We will take a look on your question and get back by this week.

    Best regards,

    Diang 

  • Hi Allen,

    It is recommended to use TPH and TPL pins as indicators of adapter input or PoE input. When SCDIS pin is open, you can enable the 50W only when TPH and TPL are both low. 

    Class 0-3 or passive injector (0 - 1 class event): TPH = Hi-Z, TPL = Hi-Z

    Class 4 (2 - 3 class event): TPH = Hi-Z, TPL = Low

    Class 5-8 (4 - 5 class event): TPH = Low, TPL = Hi-Z

    APD = High: TPH = Low, TPL = Low

    Best regards,

    Diang