Tool/software:
Hi Team,
My customer is considering to use the TPS56A37, and is looking at the application circuit setting for it.
The MODE pin of TPS56A37 is the internal fixed switching frequency setting pin which TI recommends to connect a 1% 52.3k resistor to AGND.

However, the 1% 52.3k resistor is strict. We would like to understand the reason why the 1% 52.3k resistor is required.
Although the TPS56A37 is the fixed 500kHz switching frequency, if the MODE resistor tolerance becomes wider (for example, 5%), will the switching frequency accuracy become wider too?
We would like to understand the relation between the MODE resistor tolerance and the switcihng frequency accuracy.
Best Regards,
Koshi Ninomiya