This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC38C40: DCDC Flyback design without optocoupler feedback

Part Number: UCC38C40

Tool/software:

Hi,

I'm considering to use UCC38C40 in a DCDC flyback application where there is no need for isolation. The standard flyback circuit (when used in a off-line applicaiton) involves an opto-coupler for the feedback loop to fully isolate the output from the AC input voltage.

However, in my DCDC flyback application I dont need the isolation feature and therefore I would like to remove the whole opto-coupler circuit to save cost and board space.

Now, can I simply connect the output voltage directly to the FB pin via a resistive voltage dividerm or should the signal to the somehow FB still be biased from the VREF output of UCC38C40 ?

BR

Ronny