Tool/software:
We have the same problem as described in an already existing post. A BQ79600 EVM is not answering to a sequence that should trigger an answer.
The sequence is verified on another setup with a target HW using the BQ79600. Although the BQ reacts to a COMM CLEAR ping and a request with its SPI_RDY signal it never provides the requested data. The snapshots show what's happening on the SPI seen by a logic analyzer (try with 5 MHz SPI clock) and a scope.(try with 2 MHz SPI clock).
Sequence steps:
Logic analyzer:
Scope (to check signal quality):
Silicon version: