Other Parts Discussed in Thread: UCC5881-Q1
Tool/software:
Hi Team,
Can I connect the UCC5871-Q1 driver IC to drive three parallel IGBT power modules (CM1200DW-40T)?
Each IGBT has an internal gate resistance of 0.63 Ω. Considering a driver gate voltage of 15 V, I require approximately 24 A of gate drive current per IGBT pair.
The UCC5871-Q1 provides 30 A peak current, which is sufficient for driving one module. However, for three parallel modules, we would need an additional ~60 A peak capability in total.
Could you suggest any provisions, such as external buffers, to achieve this peak current requirement for repetitive operation at up to 4 kHz?